Graphics Editor Binds and Links Pane

Use the Binds and Links pane to get an overview of the binds and links used in a graphic and their properties.

NOTE: The actual binding and linking are performed in the Graphics Editor.

Component Description
Name

Displays the name of the bind/link, consisting of the object’s name and, for the binds, a suffix normally ‘Value’. Name also shows the number of bind values or link targets that use this name. (One signal can affect several properties.)

Attribute

Displays the property (if present) that is affected by the bound value.

Format

None or Presentation. As selected in the Properties pane, under Behavior - Format.

Description

Displays an optional descriptive text.